Question
HTS221 HUMIDITY DATA CLARIFICATION
Posted on September 12, 2016 at 09:05
I am using HTS221 for humidity and temperature measurement.
On reading the registers for temperature and converting as per the equation suggested, i get the correct temperature. but on reading the registers for humidity and converting as per the equation suggested, humidity obtained is not correct. the register values read are as follows: H0_T0_OUT = 9 H1_T0_OUT = -10540 H0_RH_X2 = 53 H1_RH_X2 = 132 when humidity is measured in a controlled environment with different known humidities, the HTS221 measured humidity varies +/- 5 % within the range 26.5 % to 66% humidity(which is calibrated range of sensor), but outside the range that is lower than 26.5% and higher than 66% variation of 10 to 20% humidity is seen. kindly help to get the correct humidity. regards unnati