Question
I am curious about the power consumption of the LSM6DS3.
Posted on August 21, 2017 at 16:33
Hello.
I am curious about the power consumption of the LSM6DS3.
The LSM6DS3 can set ODR independently.
However, the power consumption when the ODR is set independently is not listed in the Application note.Only <Accelerometer only>, <Gyroscope only> and <Combo [Acc + Gyro]> are shown in Table 6.I wonder how I can calculate it.
If the Accelerometer's ODR is set to 208Hz and the Gyroscope's ODR isset to
25Hz,how much power does the sensor consume?
#output-data-rate #lsm6ds3 #power-consumption