I am trying to deploy dsh-predmnt to my personal aws account but serverless is throwing a lot of errors. I followed the PDF document "How to deploy DSH-PREDMNT in proprietary AWS account" . Is there a more detailed instruction on deploying to AWS??
PS C:\pm\predictive_maintenance_fe\serverless>node --version
v14.16.1
PS C:\pm\predictive_maintenance_fe\serverless>npm --version
7.11.1
PS C:\pm\predictive_maintenance_fe\serverless>npm install
up to date, audited 190 packages in 2s
6 packages are looking for funding
run `npm fund` for details
found 0 vulnerabilities
PS C:\pm\predictive_maintenance_fe\serverless>
PS C:\pm\predictive_maintenance_fe\serverless> serverless deploy --verbose
Serverless: Deprecation warning: Serverless Framework was enhanced with a new variables resolver which doesn't recognize "provider.variableSyntax" setting.Starting with a new major it will be the only resolver that's used.. Drop setting from a configuration to adapt to it
More Info: https://www.serverless.com/framework/docs/deprecations/#NEW_VARIABLES_RESOLVER
[dataLakeZipBuilder] lambda configured with buckets: pmsensors-weeklylake and pmsensors-ziplake
[zipFileRemover] lambda configured with bucket: pmsensors-ziplake
Serverless: Deprecation warning: CLI options definitions were upgraded with "type" property (which could be one of "string", "boolean", "multiple"). Below listed plugins do not predefine type for introduced options:
- AdditionalStacksPlugin for "skip-additionalstacks", "stack"
- Remover for "verbose"
- Assets for "verbose", "bucket"
Please report this issue in plugin issue tracker.
Starting with next major release, this will be communicated with a thrown error.
More Info: https://www.serverless.com/framework/docs/deprecations/#CLI_OPTIONS_SCHEMA
Serverless: Deprecation warning: Unresolved variable references will be communicated with a thrown error, starting from next major
More Info: https://www.serverless.com/framework/docs/deprecations/#VARIABLES_ERROR_ON_UNRESOLVED
Serverless Warning --------------------------------------
A valid file to satisfy the declaration 'file(./output.json):CDNDistributionId' could not be found.
Serverless: Configuration warning at 'functions.customResourceLambda': unrecognized property 'DependsOn'
Serverless:
Serverless: Learn more about configuration validation here: http://slss.io/configuration-validation
Serverless:
Serverless: Deprecation warning: Starting with next major, Serverless will throw on configuration errors by default. Adapt to this behavior now by adding "configValidationMode: error" to service configuration
More Info: https://www.serverless.com/framework/docs/deprecations/#CONFIG_VALIDATION_MODE_DEFAULT
Serverless: Deprecation warning: Support for "package.include" and "package.exclude" will be removed with next major release. Please use "package.patterns" instead
More Info: https://www.serverless.com/framework/docs/deprecations/#NEW_PACKAGE_PATTERNS
Serverless: Packaging service...
Serverless: WARNING: Function dataLakeZipBuilder has timeout of 900 seconds, however, it's attached to API Gateway so it's automatically limited to 30 seconds.
Serverless: Deploying additional stacks...
Serverless: Writing template for additional stack eventsQueueNestedStack...
Serverless: Creating additional stack eventsQueueNestedStack...
...
Serverless: Additional stack eventsQueueNestedStack created successfully (CREATE_COMPLETE).
Serverless: Writing template for additional stack zipBuilderNestedStack...
Serverless: Creating additional stack zipBuilderNestedStack...
......
Serverless: Additional stack zipBuilderNestedStack create failed (ROLLBACK_COMPLETE).
Error ---------------------------------------------------
Error: Additional stack zipBuilderNestedStack create failed (ROLLBACK_COMPLETE)
at C:\pm\predictive_maintenance_fe\serverless\node_modules\serverless-plugin-additional-stacks\index.js:480:37
at processTicksAndRejections (internal/process/task_queues.js:93:5)
at async PluginManager.invoke (C:\Users\chakradhar\AppData\Roaming\npm\node_modules\serverless\lib\classes\PluginManager.js:552:9)
at async PluginManager.run (C:\Users\chakradhar\AppData\Roaming\npm\node_modules\serverless\lib\classes\PluginManager.js:598:7)
at async Serverless.run (C:\Users\chakradhar\AppData\Roaming\npm\node_modules\serverless\lib\Serverless.js:313:5)
at async C:\Users\chakradhar\AppData\Roaming\npm\node_modules\serverless\scripts\serverless.js:634:9
For debugging logs, run again after setting the "SLS_DEBUG=*" environment variable.
Get Support --------------------------------------------
Docs: docs.serverless.com
Bugs: github.com/serverless/serverless/issues
Issues: forum.serverless.com