I am using a LSM6DS3, I need to receive a an interrupt signal on int1 or int2 pin which ever. When I try to set up the wake up interrupt signal as in the AN4650 chapter 4.3, it doesn't seem to trigger ever? Do you have any sample projects using this?
I search the net, and found a post with someone with a similar issue, but the link that was posted on the response is dead error 404.
I was able to set up the significant motion event to trigger on int1 but it only seems to read 1 axis of the accelerometer. And depending on its position it might never triggers the interrupt
What I would like to do is set up a "wake up" interrupt, that happens when motion is detected on any of the accelerometer axis.
Do you have any examples or sample code of this being implemented?
The one in the AN4650 never triggers no matter how i shake my board.
Thank you.
Luis.