I am using LSM303D to get accelerometer and magnetometer values but ay and az axis of accelerometer values are wrong.
I am using LSM303D to get accelerometer and magnetometer values but i keep getting ay and az axis of accelerometer values wrong. I am able to communicate with the chip because I can see the magnetometer values but something is wrong with accelerometer.
I added the picture of output values. The is as follows:
#include <Wire.h>
//Register addresses for magnetometer
#define OUT_X_L_M 0x08
#define OUT_X_H_M 0x09
#define OUT_Y_L_M 0x0A
#define OUT_Y_H_M 0x0B
#define OUT_Z_L_M 0x0C
#define OUT_Z_H_M 0x0D
// Register addresses for accelerometer
#define OUT_X_L_A 0x28
#define OUT_X_H_A 0x29
#define OUT_Y_L_A 0x2A
#define OUT_Y_H_A 0x2B
#define OUT_Z_L_A 0x2C
#define OUT_Z_H_A 0x2D
//Control Settings for LSM303D
#define CTRL0 0x1F
#define CTRL1 0x20
#define CTRL2 0x21
#define CTRL3 0x22
#define CTRL4 0x23
#define CTRL5 0x24
#define CTRL6 0x25
#define CTRL7 0x26
//Register address for gyroscope
#define OUT_X_L 0X28
#define OUT_X_H 0X29
#define OUT_Y_L 0X2A
#define OUT_Y_H 0X2B
#define OUT_Z_L 0X2C
#define OUT_Z_H 0X2D
//Control Settings for L3GD20
#define CTRL_REG1 0X20
#define MPU_HIGH_ADDR 0b0011101 // Device address of LSM303D with SDO/ADR/SA0 pulled HIGH.
#define MPU_LOW_ADDR 0b0011110 // Device address of LSM303D with SDO/ADR/SA0 connected to GND.
#define GYRO_HIGH_ADDR 0b1101011 // Device address of L3GD20 with SDO/ADR/SA0 pulled HIGH.
#define GYRO_LOW_ADDR 0b1101010 // Device address of L3GD20 with SDO/ADR/SA0 connected to GND.
#define BYTE 8
double mag_sen = 0.0000160; //magnetic sensitivity for +/- 4 gauss in gauss/LSB units
double acc_sen = 0.0000610; //linear acc sensitivity for +/- 2G in G/LSB units
double gyro_sen = 0.008750;
int16_t mx,my,mz;
int16_t ax,ay,az;
int16_t gx,gy,gz;
void setup(){
Serial.begin(9600);
Serial.println("Serial Begin");
Wire.begin();
enableDefault();
delay(250);
}
void loop(){delay(1000);
mx = (int16_t)readRegister(OUT_X_H_M)<<BYTE | readRegister(OUT_X_L_M);
my = (int16_t)readRegister(OUT_Y_H_M)<<BYTE | readRegister(OUT_Y_L_M);
mz = (int16_t)readRegister(OUT_Z_H_M)<<BYTE | readRegister(OUT_Z_L_M);
Serial.print("Mag: ");
Serial.print(mx*mag_sen,DEC);Serial.print("\t");
Serial.print(my*mag_sen,DEC);Serial.print("\t");
Serial.print(mz*mag_sen,DEC);Serial.print("\t");
ax = (int16_t)readRegister(OUT_X_H_A)<<BYTE | readRegister(OUT_X_L_A);
ay = (int16_t)readRegister(OUT_Y_H_A)<<BYTE | readRegister(OUT_Y_L_A);
az = (int16_t)readRegister(OUT_Z_H_A)<<BYTE | readRegister(OUT_Z_L_A);
Serial.print("Acc: ");
Serial.print(ax*acc_sen,DEC);Serial.print("\t");
Serial.print(ay*acc_sen,DEC);Serial.print("\t");
Serial.print(az*acc_sen,DEC);Serial.print("\t");
gx = (int16_t)readReg(OUT_X_H)<<BYTE | readReg(OUT_X_L);
gy = (int16_t)readReg(OUT_Y_H)<<BYTE | readReg(OUT_Y_L);
gz = (int16_t)readReg(OUT_Z_H)<<BYTE | readReg(OUT_Z_L);
Serial.print("Gyro: ");
Serial.print(gx*gyro_sen,DEC);Serial.print("\t");
Serial.print(gy*gyro_sen,DEC);Serial.print("\t");
Serial.print(gz*gyro_sen,DEC);Serial.println();
}
void enableDefault(){
writeRegister(CTRL0,0x00);
//Accelerometer settings
//0x37 = 0b00110111
//AODR = 0011 (12.5 Hz)
writeRegister(CTRL1,0x37);
//Full-scale selection = +/- 2g
writeRegister(CTRL2,0x00);
//Magnetometer Settings
// 0x68 = 0b01101000
//M_RES = 11 (high resolution), M_ODR = 010 (12.5 Hz)
writeRegister(CTRL5,0x68);
//MD = 00 (the device does conversions repeatedly)
writeRegister(CTRL7,0x00);
//Gyroscope Settings
//0x2F = 0b00101111
writeReg(CTRL_REG1,0x2F);
}
int8_t readRegister(int8_t reg){
int8_t buffer;
Wire.beginTransmission(MPU_HIGH_ADDR);
Wire.write(reg);
Wire.endTransmission(0); //sends restart message so the bus will not be released
Wire.requestFrom(MPU_HIGH_ADDR,1);
while(Wire.available() == 0);
buffer = Wire.read();
Wire.endTransmission(1);
return buffer;
}
void writeRegister(int8_t reg, int8_t val ){
Wire.beginTransmission(MPU_HIGH_ADDR);
Wire.write(reg);
Wire.write(val);
Wire.endTransmission();
}
void writeReg(int8_t reg, int8_t val){
Wire.beginTransmission(GYRO_HIGH_ADDR);
Wire.write(reg);
Wire.write(val);
Wire.endTransmission();
}
int8_t readReg(int8_t reg){
int8_t buffer;
Wire.beginTransmission(GYRO_HIGH_ADDR);
Wire.write(reg);
Wire.endTransmission(0);
Wire.requestFrom(GYRO_HIGH_ADDR,1);
while(Wire.available() == 0);
buffer = Wire.read();
Wire.endTransmission(1);
return buffer;
}