Question
I am working on a design in STM32CubeIDE that uses the STM32L053 connecting to four sensors connected over I2C. I am trying to use the examples from the https://github.com/STMicroelectronics/STMems_Standard_C_drivers repo.
For example, the HTS221 sensor responds correctly to the "WhoAmI" query. It then responds with a NAN when trying to read the temperature or the humidity. Some of the other drivers do not even respond to the "WhoAmI" command correctly. Would using these drivers be the correct approach, or is there some other preferred method?