I can't enter the decimal part of a number in to the Converter field in MEMS-studio.
Hello,
I want to enter the decimal part of a number in to filed "Float" (Advanced Features -> FSM -> Converter).
The Decimal Separator in the Regional Settings of the system I use (KDE/plasma) is a comma.
It seems that the "Float" field only accepts a decimal point as decimal separator, but I cannot enter the decimal point character in this field: after pressing "." key nothing appears in this field.
I can enter the "," character as decimal separator, but after conversion I get the wrong result in the field "Float16".
Am I missing a some option in MEMS-studio settings to solve this problem?
Additional info: if the "Float" field already contains a decimal point, I can enter "." character, but if the field was initially empty, then I can't enter "." character.
P.S. I remember I had the same problem on Windows and in the previous version of MEMS-studio.
MEMS-studio v1.3.0
My system:
Operating System: Arch Linux
KDE Plasma Version: 6.1.2
KDE Frameworks Version: 6.3.0
Qt Version: 6.7.2
Kernel Version: 6.6.37-1-lts (64-bit)
Graphics Platform: X11
Processors: 16 × AMD Ryzen 7 1700X Eight-Core Processor
Memory: 62.7 GiB of RAM
Graphics Processor: NVIDIA GeForce GTX 1080 Ti/PCIe/SSE2