I can't use MEMS-studio under KDE/Plasma (linux)
Hello,
in KDE/plasma environment I can't use MEMS-studio because it doesn't show file dialogs.
For example: MEMS-studio is connected to the STEVAL-MKI109V3 board, in "Advanced Features" -> "FSM" I click the "Load state machine from file“ button, but nothing happens, the file dialog does not appear.
Is there any solution to allow MEMS-studio to work properly in the KDE/plasma environment?
When I run MEMS-studio from the command line I get this output from the console:
Searching in: "/home/senbuvis/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin"
Searching in: "/home/senbuvis/STMicroelectronics/STM32CubeProgrammer/bin"
Searching in: "/home/senbuvis/STMicroelectronics/STM32Cube/bin"
Searching in: "/home/senbuvis/STMicroelectronics/bin"
Searching in: "/opt/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin"
Searching in: "/opt/STMicroelectronics/STM32CubeProgrammer/bin"
Searching in: "/opt/STMicroelectronics/STM32Cube/bin"
Searching in: "/opt/STMicroelectronics/bin"
Searching in: "/usr/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin"
Searching in: "/usr/STMicroelectronics/STM32CubeProgrammer/bin"
Searching in: "/usr/STMicroelectronics/STM32Cube/bin"
Searching in: "/usr/STMicroelectronics/bin"
Searching in: "/usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin"
Searching in: "/usr/local/STMicroelectronics/STM32CubeProgrammer/bin"
Searching in: "/usr/local/STMicroelectronics/STM32Cube/bin"
Searching in: "/usr/local/STMicroelectronics/bin"
Searching in: "/home/senbuvis/ST/STEdgeAI/1.0/Utilities/linux"
Searching in: "/opt/ST/STEdgeAI/1.0/Utilities/linux"
Searching in: "/usr/ST/STEdgeAI/1.0/Utilities/linux"
Searching in: "/usr/local/ST/STEdgeAI/1.0/Utilities/linux"
void DeviceManagerInterface::setIsBusy(bool) false false
void AfsManager::initParamsToDefault()
file:///home/senbuvis/Poligonas/MEMSstudio_1.3.0/opt/mems-studio/qml/QtQuick/Dialogs/DefaultFileDialog.qml:413:17: QML ToolButton: Binding loop detected for property "implicitHeight"
file:///home/senbuvis/Poligonas/MEMSstudio_1.3.0/opt/mems-studio/qml/QtQuick/Dialogs/DefaultFileDialog.qml:309:21: QML Button: Binding loop detected for property "implicitHeight"
file:///home/senbuvis/Poligonas/MEMSstudio_1.3.0/opt/mems-studio/qml/QtQuick/Dialogs/DefaultFileDialog.qml:309:21: QML Button: Binding loop detected for property "implicitHeight"
qml: OS DETECTED: linux
plugin.communication:
app.monitoringDataModel:
mems-studio Started, processing run parameters..
I'm using MEMS-studio v1.3.0.
My system specs:
Operating System: Arch Linux
KDE Plasma Version: 6.1.1
KDE Frameworks Version: 6.3.0
Qt Version: 6.7.2
Kernel Version: 6.6.36-1-lts (64-bit)
Graphics Platform: X11
Processors: 16 × AMD Ryzen 7 1700X Eight-Core Processor
Memory: 62.7 GiB of RAM
Graphics Processor: NVIDIA GeForce GTX 1080 Ti/PCIe/SSE2