I'm looking for an equivalent to the LOPS33W sea water compatible pressure sensor, but with 2 and 4 ATM (and possibly higher) absolute full scale ranges.
The digital IO of pressure and temperature is nice, but we can also use an analog output. The digital is good for a new high volume project, but we need an analog output for a current application. Small size and low power requirements are also important as the instruments are portable and battery powered for extended periods.
Depending on the specific application, the environment exposes the sensor pressure input to sea water, industrial cooling water, and the stomach contents of cattle...rather a wide range but very challenging for an un-protected sensor.