Skip to main content
Visitor II
December 5, 2019
Question

I'm using a LSM9DS1. I find that the datasheet gives a good functional description of the accelerometer and gyroscope, but it only gives register level information for the magnetometer. Is there a datasheet for the compass as a stand-only part?

  • December 5, 2019
  • 2 replies
  • 772 views

The datasheet also refers to self test modes, but no explanations are given.

    This topic has been closed for replies.

    2 replies

    ST Employee
    December 10, 2019

    Hi @NathanCrow​ , a reference datasheet for the magnetic part of the LSM9DS1 is the LIS3MDL (same sensitivity and full scale). Specifically for the self test, I suggest you the AN5069 p.23 and 24 (LIS2MDL has register in 60h range instead of 20h range; and different performances). Regards

    Visitor II
    December 10, 2019

    Thank you very much. These documents are quite helpful.

    Would I be correct to assume that the RMS noise numbers are in a 40 Hz band (ODR/2 = 80/2) and that they would be the same at FS=+/- 4 Gauss?

    ST Employee
    December 11, 2019

    Right, but take care of the offset that is not small hand has to be measured and subtracted to the acquired data. It doesn't directly affect the rms noise however. Regards