I'm using the LIS3DH. Do I need to provide a 90 mS delay between configuration of CTRL_REG1 and reading the OUT registers or the FIFO to insure stable output ?
I'm using the LIS3DH. The Application Note AN3308 specifies a 90 mS delay time between configuration and reading data in the suggested procedure for performing a self test, (p57 of DocID18198 Rev 3). The delay is, "... for stable output". Once ODR is set or FIFO enabled, is a delay required to insure stable data? If so, how long of a delay is adequate? 90 mS eats up a lot of power while the LIS3DH is just sitting there. Would 5 mS or 0 mS be OK?