Question
I was wondering how can I set interrupt threshold value in IG_THS_X1 /Y1/Z1 register.
I am using LIS2HH12 accelerometer. In threshold register do I need to write value in terms of g. If I need to set threshold as 0.4 g then how to write .suppose if I want to set +0.4 (or -0.4) , writing 0.4 (float value) in 1 byte is not possible. Any conversion formulae I need use. Please help.