Skip to main content
Visitor II
November 30, 2021
Solved

IIS2DH aliasing at low ODR settings

  • November 30, 2021
  • 4 replies
  • 1245 views

AFAIK the IIS2DH has no anlog anti aliasing filter. So will aliasing occure if I use low ODR settings and the input signal is frequency is higher than ODR/2? Because in our test we are getting quiten often spikes in the signal output signal.

And if this is the case we could only crank up the sampling rate?

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @THart.14​ ,

    A little aliasing effect will probably occur, but the folded signal should be very attenuated.

    This is for example the frequency response of the Z axis, that shows that the signal is very attenuated above 2kHz (which is half of the maximum ODR setting, Low-power mode (5.376 kHz)).

    0693W00000GZfkYQAT.png 

    -Eleon

    4 replies

    ST Employee
    December 1, 2021

    Hi @THart.14​ ,

    A little aliasing effect will probably occur, but the folded signal should be very attenuated.

    This is for example the frequency response of the Z axis, that shows that the signal is very attenuated above 2kHz (which is half of the maximum ODR setting, Low-power mode (5.376 kHz)).

    0693W00000GZfkYQAT.png 

    -Eleon

    THart.14Author
    Visitor II
    December 2, 2021

    Thx, for your response.

    But at lower ODR settings the chip will use lower ADC sampling rates eg at ODR=200Hz or 400Hz, thus this will lead to aliasing effects?

    THart.14Author
    Visitor II
    December 7, 2021

    Please could you clarify that in the case not properly low pass filtered input acceleration data the only way to avoid aliasing is to set ODR to 5376Hz?

    ST Employee
    December 9, 2021

    Hi @THart.14​ ,

    for lower than maximum ODR there is a low risk of aliasing folding, but the signal will be very attenuated.

    -Eleon