IIS2DH Anti-Aliasing Low Pass Filter by Design in comparison to IIS3DWB and what are the resonance frequencies of each axis of the IIS2DH?
Hi,
so far we want to compare several MEMS accelerometers and their specifications. From ST, two sensors are on our list, the IIS3DWB and the IIS2DH.
For the IIS3DWB, the data sheet offers a frequency response curve at page 19 and regarding aliasing the following information (see IIS3-Block-Diagram-Frequency-Response.PNG):
"The IIS3DWB has been specifically designed to provide a wide bandwidth with very flat frequency response in the
pass band and a very high attenuation in the stop band so to virtually eliminate any frequency aliasing."
1) So for the IIS3DWB their is no "true" analog low pass filter before the ADC in order to prevent aliasing, its simply done by the frequency response of the senor itself right? Because the LPF1 is a digital low pass filter, in theory not capable of preventing aliasing effects.... Or am i on a wrong direction :) ?
2) Does the frequency response for the IIS2DH provides a low pass curve progression by the sensor itself too in order to eliminate aliaising, simillar to the IIS3DWB?
The IIS3DWB on page 5 offers the following information about the resonance frequency for each axis (see IIS3-Axis-Resonance-Frequencies.PNG).
3) What is the resonance frequency for the axis of the IIS2DH?
Hope my questions are correctly written, because I am not a native english speaker. Thanks for your help.
Greetings,
Joe
PS: for me, it was not possible to add inline pictures (error: "Object of InlineImage message segment is missing expected property...") ;) maybe i did something wrong or its an issue while submitting...