IIS2DH Reading FIFO
With a 2g scale sampling @25Hz the FIFO fills with data and I am reading the contents up to the watermark. HR and LPen are disabled.
With the Z-Axis pointing toward earth I get the following data for the X-Axis using the H and L bytes:
DATX=128
DATX=128
DATX=128
DATX=-64
DATX=192
DATX=-128
DATX=-64
DATX=0
...
First, why are the values multiples of 32? Second, why the variability when the chip is still and not moving? I have been using the LIS3DSH for a couple years now so this IIS2DH is a real downgrade for sure, but I must be missing something. I have read over the manual several times now and can't find my issue.
-AP