IIS2DLPC Threshold Interrupt
Coming from the IIS2DH which had a simple threshold interrupt by axis that worked great.
Can we achieve a similar thing with the IIS2DPLC? Specifically I want to do the following:
If an axis exceeds a threshold value it will persist an output (INT1 or INT2) line until the acceleration value is below the threshold.
I have tested the wake / sleep functionality successfully, but it seems the high pass filter is on by default? I say this because even if the threshold is exceeded and the wake event occurs, the sleep event will also eventually occur even if the value still exceeds the threshold.