IIS2DLPC wake up interrupt bit always set?
it seems that the status bits in the registers for wake up are always active - Is it possible to remove them?
If I setup the part to wake up routing the wake up to INT1, then issue a soft reset to the device, setting it up next to just route the DRDY to INT1 ,it the wake_up_src.wu_ia bit is always set no matter what -Is it possible not to have the wakeup functionality active? (or am I missing something that a soft reset isn't doing to disable those bits in the register). Thanks