Skip to main content
Visitor II
June 29, 2024
Question

IIS2DLPCTR ODR Accuracy

  • June 29, 2024
  • 1 reply
  • 1030 views

Could you please provide information about the output data rate (ODR) for the IIS2DLPCTR accelerometer?

For example, if I want an ODR of 50Hz in High Performance mode, with BW=ODR/2, how accurate is the 50Hz ODR?  Similarly, if I use the single data conversion on-demand mode at 50Hz, what would the accuracy be (assuming a perfect 50Hz trigger on INT2)?

 

Thanks.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    July 4, 2024

    Hi @NBerr.1 ,

    From characterization measurements the ODR accuracy of IIS2DLPCTR is +/- 15%, note that it is tested on a limited number of samples and thus not guaranteed in production.

    NBerr.1Author
    Visitor II
    July 4, 2024

    Thanks Federica. When using ‘single data conversion on-demand mode’, how accurate is the actual sampling of the MEMS device relative to  the trigger signal on INT2?  In this case I’m not referring to T_on. I’m more interested in how ‘true’ the sample time is in this mode. In other words, if I  have a rising edge on INT2 to request a sample, how much internal delay will there be before the part’s internal ADC takes a sample?

     

     

     

    NBerr.1Author
    Visitor II
    July 5, 2024

    For this, I am assuming the case where SLP_MODE_SEL = 0.