Skip to main content
Visitor II
September 30, 2019
Question

IIS2MDCTR temperature rating.

  • September 30, 2019
  • 1 reply
  • 585 views

Please present the junction temperature rating of IIS2MDCTR,

Is it generally the same as the storage temperature?

    This topic has been closed for replies.

    1 reply

    ST Employee
    October 4, 2019

    Hi @HTaka.8​ , please check if I well interpreted you question. The IIS2MDCTR max supply is 3.6V and max current (high performance mode, max ODR) is 1130uA, so the power consumed in the worst case is P=V*I=4mW. If you consider that the device package thermal resistance is 80°C/W, the thermal difference between the device and the environment is DeltaT=0.3°C worst case. Moreover, no worry about the junction temperature with respect to storage temperature. Regards