Skip to main content
Visitor II
October 10, 2018
Question

IIS328DQ will this accelerometer works for slow movements or constant movements?

  • October 10, 2018
  • 4 replies
  • 902 views

My Requirement:

I want to get the data if there is a angle change more than 5 degrees in any direction(X , Y , Z) 

 and it should work for very slow movements or linear or constant movements. Will this sensor works as per my requirement or not. Please suggest me suitable one if it is not.

 Thanks in advance. 

Sensor : IIS328DQ (accelerometer) 

    This topic has been closed for replies.

    4 replies

    ST Employee
    October 24, 2018

    Will the starting position be given and always the same?

    Or do you want to detect the angle change from any staring position?

    RKuma.17Author
    Visitor II
    October 24, 2018

    I want to detect the angle change from any starting position...

    ST Employee
    October 24, 2018

    It is not possible to achieve this functionality with embedded sensor features. A microcontroller is needed to do it. You also have to determine a minimum speed which should be detected.

    RKuma.17Author
    Visitor II
    October 24, 2018

    So i need to set the speed in the sensor to achieve this right?