IIS3DWB bandwidth
Hi,
The LPF2 filter on the IIS3DWB can set the cutoff frequency to ODR/4, ODR/10, ODR/20, etc. Figure 6 in the datasheet "Frequency response with LPF2 enabled" shows the bandwidth when LPF2 is set to ODR/4 to be 5.6 kHz. Is this correct? ODR/4 would put the cutoff at 26.67 kHz / 4 = 6.67 kHz. Does "ODR/4" simply describe the LPF2 stage and not the actual resulting bandwidth?
Thanks for your help,
Steve