IIS3DWB power consumption in wait-for-event
Hello,
IIS3DWB documentation provides only two data points about power consumption:
Accelerometer current consumption @ 1.1mA typ.
Accelerometer current consumption during power-down @ 5µA typ.
I want to be woken-up on vibration levels (on X, Y or Z axis) when a specific threshold gets crossed. The datasheet provides all information about how to do that. However I miss the µA targets. I understand that ODR is fixed anyway @ 26.6667 kHz but I m guessing that power consumption should be well below the nominal 1.1.mA. My target is in the tens of µA to 100 µA range maximum. Else I need a second accelerometer to provide the function.
Note: I can cut VDDIO during such mode (VDDIO distinct from VDD) but still need INT1 event toward my microcontroller.
Can you provide typical power consumption in such mode so that I can finalize my architecture.
Thanks
Best Regards,
Stephane