Skip to main content
Visitor II
October 16, 2025
Question

IIS3DWB use ST sample code to polling, Acceleration value significant differences in changes

  • October 16, 2025
  • 1 reply
  • 223 views

Dear ST Mems,

Customer Shenzhen Vtech uses IIS3DWB for water pipe vibration detection, using the official routine SPI polarization detection. The data read varies greatly.
Revise as follows:
1: Communicate with R&D team to conduct self inspection first, pass the self inspection, and then poll. However, there is still a lack of contact, fixed placement, and large deviation in the sampling process.
2: Modify the range. Switch from the initial+-2g to+-4g, without contact, with fixed placement and large variation deviation during the sampling process.
3: Using a DC stabilized power supply to ensure stable power supply for IIS3DWB, the issue has not been resolved.
The following are pictures of product placement and logo information for sampling. May I ask where specific modifications can be made to address the issue of significant numerical variations during the sampling process. Thank you!

mmexport1760595492196.jpgmmexport1760595499895.jpg

    This topic has been closed for replies.

    1 reply

    ST Employee
    October 17, 2025

    YUFENGLI

     

    This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

     

    Regards

    Joe

    STMicro Support