IIS3DWB uses ~275uA in Low power mode - not 5uA-16uA
I have an issue with current consumption of a IIS3DWB using the STEVAL-MKI208V1 kit.
I have previously discussed it in this issue, but I've traced (i hope) the issue to the VDDIO pin.
I'm using a STM32WB55CEU6 as SPI master.
To measure current I'm using the X-Nucleo-LPM01A.
When the ISS3DWB is in low-power mode it should use 5-16uA, but I'm measuring ~265uA.
Schematic:

Measurement of ONLY the STEVAL-kit VDD-pin (ISS3DWB in Low-power - VDDIO pin connected to MCU VDD):
Measurement of the STEVAL-kit VDDIO-pin (ISS3DWB in Low-power - VDD pin connected to MCU VDD):
Measurement of STEVAL-kit VDD + VDDIO in low-power-mode
I'm not sure I understand why VDDIO is drawing so much current - isn't it supposed to be the SPI voltage reference?
Any ideas?
Regards