IKS4A1 eCompass application with Unicleo-GUI
Hello, I am trying to test the e-compass application with the IKS4A1 connected to a Nucleo-F446 and Unicleo-GUI.
The firmware of the Nucleo F446 was produced from Cube-MX following the "Getting started with the STMicroelectronics X-CUBE-MEMS1 software package for STM32MX".
For some unexplainable (to me) reason, it looks like the board looks for sensors placed on another expansion board I don't have so that I am unable to get sensor data from the magnetometer placed on the IKS4A1.
The IKS4A1 magnetometer is placed on the right side of the board. I have not the green board shown in the picture and it seems to me I have not configured it.

When I open Unicleo the user message tab shows:
Port: COM8 Successfully Opened
PresString Received: MEMS shield demo,12,10.0.0,1.5.0,IKS4A1
Firmware Type: E-Compass
Expansion Board IKS4A1 Successfully Initialized
but nothing works.
Here my Cube project.
Any help will be very appreciated.
Thank you.