ILPS28QSW o-ring
Hi,
I'm having a hard time to find a supplier for an o-ring to get the ILPS28QSW sensor waterproof.
In AN5937 ST mentioned they use an o-ring with: ID 1.8mm, thickness 0.5mm (see picture below)
Does anyone here know any supplier who make these, or have used another size with good results? For example if a thickness of 0.75mm would work? I'm afraid the o-ring might be to big?
And FYI: The cylinder formed hole for the sensor is very similar to the one ST is using in AN5937
O-ring from AN5937:

Dimensions of the ILPS28QSW from the datasheet: