Incoherence between LSM6DSL, LSM6DSO and ISM330DHCX datasheets and Application Notes
Hello,
I noticed some incoherence between the documentations of the LSM6DSL, LSM6DSO and ISM330DHCX concerning the value of the last 3 ODR of the sensors.
- LSM6DSL Datasheet : 1666Hz - 3332Hz - 6664Hz
- LSM6DSL AN5040 : 1666Hz - 3333Hz - 6666Hz
- LSM6DSO Datasheet : 1666Hz - 3332Hz - 6664Hz
- LSM6DSO AN5192 : 1667Hz - 3333Hz - 6667Hz
- ISM330DHCX Datasheet : 1666Hz - 3332Hz - 6667Hz
- ISM330DHCX AN5398 : 1667Hz - 3333Hz - 6667Hz
Which frequencies should we consider ?
Thank you,
Best regards,
Clotilde