Skip to main content
Visitor II
January 16, 2011
Question

iNemo STEVAL-MKI062V2 AHRS Mode

  • January 16, 2011
  • 4 replies
  • 1546 views
Posted on January 16, 2011 at 07:31

This board supports an ''AHRS'' mode, but on my computer the option is grayed out. I am running V2 of the board which is supposed to support this mode. Is there some addional firmware that must be loaded? If so, where do I get it and how do I load it?

Thanks

Al
    This topic has been closed for replies.

    4 replies

    Visitor II
    January 18, 2011
    Posted on January 18, 2011 at 11:03

    Hi Al,

    Probably firmware upgrading is necessary, here below the procedure:

    1. Download and install the Dfuse from  the URL: 

      http://www.st.com/internet/evalboard/product/250367.jsp

    2. Run the DFU demo application
    3. Start the device in DFU mode --> Plug in the USB cable pressing the button (SW2)
    4. The device is recognized as a DFU device. Select the iNEMOV2_Firmware_PackageV2.0.0_AHRS.dfu file from installation folder of the iNEMOâ„¢ suite application under the Firmware/DFU image folder and upgrade
    5. Press Leave DFU mode

    6. Check the Device Manager now. In ports, you should now find the STEVAL-MKI062V2 device connected
    7. Run the iNEMOâ„¢ application
    Details are available in the User Manual UM0993 at

    http://www.st.com/inemo

    .

    Best Regards

    iNEMOâ„¢ Team

    Visitor II
    January 25, 2011
    Posted on January 25, 2011 at 11:17

    Hi Fabio

    I upgraded my iNemo STEVAL-MKI062V2 with the file ''iNEMOV2_Firmware_PackageV2.0.0_AHRS.dfu'', but the AHRS stays greyed out in the iNemo Suite GUI, any reason why we can't use the AHRS mode ?

    Regards

    Philip

    Visitor II
    January 26, 2011
    Posted on January 26, 2011 at 15:06

    Hi Philip,

    First, check about correct upgrading of firmware trought Help>About menu of Suite (with the board connected).

    Below the versions of Suite Ver.2.0.0, as reference:

    ControlLibrary Ver. 2.0.04

    ControlLibrary.MKI062V2 Ver. 2.0.0

    iNEMO 2 SDK for STEVAL-MKI062V2 Ver. 1.6.0

    TL_002 Frame Transport Layer Ver. 1.0.0

    PL_001 Dynamic Link Library Ver. 1.1.2

    Firmware :iNEMO Firmware_Version_2.0.0 - iNEMO AHRS ENABLE V1.2.0

    Hardware :iNEMO V2 Hardware_Version_1

    After, you kindly follow this simple sequence:

    1)

    Connect the board to USB

    2)

    Open the Suite and connect the board to the virtual COM (pag.8 of attached UM1010)

    3)

    Push the

    Connect Icon the communication between Suite and Board(fig.10)

    4)

    Set the acquisition mode to AHRS from

    Tools>Communication>Mode(pag.12)

    5)

    Select the acquisition mode (sample/continuous) and push the

    Play Icon

    6)

    Now all is ready for launch the 3D Demo cube in AHR mode

    Best Regards

    Fabio

    ________________

    Attachments :

    UM1010.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzYJ&d=%2Fa%2F0X0000000bNX%2FUPRZyKrJbrnDG7UnLhCTFgsVszah1qZOFh4il4JfbmU&asPdf=false
    Visitor II
    January 27, 2011
    Posted on January 27, 2011 at 08:30

    Thanks Fabio

    Everything  is working now!

    You need to be connected BEFORE you can change the mode !!

    Philip