Question
Inprove the speed of the ''Mass storage'' as u disk
Posted on March 13, 2012 at 09:30
hello everybody,
I was tested using the TF card as a U disk routines.The read speed is 500KB-700KB / s, write speed of 100KB/ s. Too slow, I would like to increase its transmission speed.I will change the way of the USB to transfer data to double buffering, speed does not improve, I would like to speed transmission bottlenecks on the TF card flash, and do you have any good suggestions?(In this post I willcontinue to update content on the USB.) (The operation of the TF card SDIO,DMA, 4bit.) #usb-sdio-tf-card #usb-tf-dma-sdio #usb-tf-card-sdio