Is LSM6DSL zephyr driver compatible with LSM6DSR ?
Hi,
I am trying to create test the STEVAL-MKI194V1 for a test vehicle, which has LSM6DSR. However, I do not get an initialization response from it using the Zephyr device tree. So, I did a test (without the DSL driver) with the spi shell which gives me the correct chip ID output. Is the DSL driver compatible with the DSR? OR would I need a separate driver for both ?
Thanks,
Devang