Is There a Dedicated Android Library for Interfacing with STHS34PF80 Proximity Sensor?
Hi,
I am currently working on a project using the STHS34PF80 proximity sensor from STMicroelectronics. The platform is running Android 14.0.0_1.0.0 (L6.1.55_2.2.0 BSP).
I would like to know if there is a dedicated Android driver or SDK available to directly interface with the STHS34PF80 sensor—either from STMicroelectronics or open-source contributors.
I have the datasheet and application notes for the sensor, and I understand its I²C communication protocol. However, before starting from scratch, I’d like to ask:
1) Any existing Android libraries or HAL implementations
2) Sensor integration examples in Android (preferably for NXP i.MX8M Plus - based platforms)
Any examples or references would be greatly appreciated.
Thanks in advance for your support!