Is there any method to use en.fp-sns-allmems1 on the the sensor tile indipendetly from BLE application?
Good afternoon,
I would like to use the Sensor tile on which is running the en.fp-sns-allmems1 fw to directly record sensor measurements on the SD card. The idea is to power on the sensor tile, then dobletapping on the sensor tile to start recording directly on the SD card; once I dobletapping on the sensor tile, it stops recording on SD. In a nutshel, I want en.fp-sns-allmems1 to work like en.stsw-stlkt01 on the sensor tile without interacting with the BLE app, because I am interested in having quaternions recorded in csv and en.stsw-stlkt01 does not support quaternions. Should I try to (a) adapt en.fp-sns-allmems1 to do as I said above or should I try to include a library for computing and recording quaternions in en.stsw-stlkt01? If it is better to do (b) what library do you suggest ?
Since I am new to programming at these level could you provide me some hints and examples, please ?