Skip to main content
Graduate II
March 27, 2025
Question

ISM330DLC : How to properly set FIFO

  • March 27, 2025
  • 1 reply
  • 506 views

Hi,

I am really new to this sensor and I was able to get the polling mode working.

I am planning for full 6.6k odr rate and FIFO samples can be 256 when INT1 should be triggered or whenever possible so I can use FIFO .

I am really confused with the order / things to keep in mind to properly get this working. I am using steval Idp0051v which has ISM330DLC sensor connected via SPI1 .

This is my code that hass all the functions to use the sensor :

/*
 * memsSensor.c
 *
 * Created on: Mar 26, 2025
 * Author: amrith
 */


#include "memsSensor.h"
#include "ism330dlc.h"
#include "main.h"

extern SPI_HandleTypeDef hspi1;

ism330dlc_ctx_t ism330dlc_ctx = {
 .write_reg = ism330dlc_spi_write,
 .read_reg = ism330dlc_spi_read,
 .handle = NULL // Not used in this case, but can point to &hspi1 if needed
};


// IO structure for ism330dlc.h
ISM330DLC_IO_t ism330dlc_io = {
 .Init = ISM330DLC_SPI_Init,
 .DeInit = ISM330DLC_SPI_DeInit,
 .BusType = ISM330DLC_SPI_4WIRES_BUS, // Using SPI 4-wire mode
 .Address = 0x00, // Not used for SPI
 .WriteReg = ISM330DLC_SPI_WriteReg,
 .ReadReg = ISM330DLC_SPI_ReadReg,
 .GetTick = ISM330DLC_GetTick
};


// Object structure
ISM330DLC_Object_t ism330dlc_obj;


// Previous data for change detection
static ISM330DLC_Axes_t prev_accel_data = {0, 0, 0};
static ISM330DLC_Axes_t prev_gyro_data = {0, 0, 0};

// FIFO buffer and variables
#define FIFO_WATERMARK 100 // Number of samples to trigger interrupt (max 512)
#define FIFO_SAMPLE_SIZE 12 // 6 bytes accel + 6 bytes gyro per sample
static uint8_t fifo_buffer[FIFO_WATERMARK * FIFO_SAMPLE_SIZE]; // Buffer for FIFO data
static volatile uint8_t fifo_data_ready = 0; // Flag for ISR


// SPI read implementation
int32_t ism330dlc_spi_read(void *handle, uint8_t reg, uint8_t *data, uint16_t len) {
 HAL_GPIO_WritePin(ISM330DLC_CS_PORT, ISM330DLC_CS_PIN, GPIO_PIN_RESET); // CS low
 reg |= 0x80; // Set read bit (MSB = 1 for read)
 if (HAL_SPI_Transmit(&hspi1, &reg, 1, HAL_MAX_DELAY) != HAL_OK) {
 HAL_GPIO_WritePin(ISM330DLC_CS_PORT, ISM330DLC_CS_PIN, GPIO_PIN_SET); // CS high
 return -1; // Error
 }
 if (HAL_SPI_Receive(&hspi1, data, len, HAL_MAX_DELAY) != HAL_OK) {
 HAL_GPIO_WritePin(ISM330DLC_CS_PORT, ISM330DLC_CS_PIN, GPIO_PIN_SET); // CS high
 return -1; // Error
 }
 HAL_GPIO_WritePin(ISM330DLC_CS_PORT, ISM330DLC_CS_PIN, GPIO_PIN_SET); // CS high
 return 0; // Success
}

// SPI write implementation
int32_t ism330dlc_spi_write(void *handle, uint8_t reg, uint8_t *data, uint16_t len) {
 HAL_GPIO_WritePin(ISM330DLC_CS_PORT, ISM330DLC_CS_PIN, GPIO_PIN_RESET); // CS low
 reg &= 0x7F; // Clear read bit (MSB = 0 for write)
 if (HAL_SPI_Transmit(&hspi1, &reg, 1, HAL_MAX_DELAY) != HAL_OK) {
 HAL_GPIO_WritePin(ISM330DLC_CS_PORT, ISM330DLC_CS_PIN, GPIO_PIN_SET); // CS high
 return -1; // Error
 }
 if (HAL_SPI_Transmit(&hspi1, data, len, HAL_MAX_DELAY) != HAL_OK) {
 HAL_GPIO_WritePin(ISM330DLC_CS_PORT, ISM330DLC_CS_PIN, GPIO_PIN_SET); // CS high
 return -1; // Error
 }
 HAL_GPIO_WritePin(ISM330DLC_CS_PORT, ISM330DLC_CS_PIN, GPIO_PIN_SET); // CS high
 return 0; // Success
}




// Higher-level IO implementations
int32_t ISM330DLC_SPI_Init(void) {
 return ISM330DLC_OK; // SPI1 already initialized by CubeMX
}

int32_t ISM330DLC_SPI_DeInit(void) {
 return ISM330DLC_OK; // No de-init needed
}

int32_t ISM330DLC_SPI_WriteReg(uint16_t Addr, uint16_t Reg, uint8_t *pData, uint16_t Length) {
 return ism330dlc_write_reg(&ism330dlc_ctx, (uint8_t)Reg, pData, Length);
}

int32_t ISM330DLC_SPI_ReadReg(uint16_t Addr, uint16_t Reg, uint8_t *pData, uint16_t Length) {
 return ism330dlc_read_reg(&ism330dlc_ctx, (uint8_t)Reg, pData, Length);
}

int32_t ISM330DLC_GetTick(void) {
 return HAL_GetTick();
}


void ISM330DLC_Setup(void) {
 // Register the IO functions
 if (ISM330DLC_RegisterBusIO(&ism330dlc_obj, &ism330dlc_io) != ISM330DLC_OK) {
 // Handle error
 while (1);
 }

 // Link the low-level context
 ism330dlc_obj.Ctx = ism330dlc_ctx;

 // Initialize the sensor
 if (ISM330DLC_Init(&ism330dlc_obj) != ISM330DLC_OK) {
 // Handle error
 while (1);
 }

 // Verify device ID
 uint8_t device_id;
 if (ISM330DLC_ReadID(&ism330dlc_obj, &device_id) != ISM330DLC_OK || device_id != ISM330DLC_ID) {
 // Handle error (ISM330DLC_ID = 0x6A)
 while (1);
 }
}



void ISM330DLC_ConfigureFIFO(void) {

	 if (ISM330DLC_FIFO_Set_Mode(&ism330dlc_obj, ISM330DLC_STREAM_MODE) != BSP_ERROR_NONE)
	 {
	 ret = -1;
	 }

 if (ISM330DLC_FIFO_Set_INT2_FIFO_Full(&ism330dlc_obj, ENABLE) != BSP_ERROR_NONE)
 {
 ret = -1;
 }
 // Verify
 uint8_t reg_val;
 ism330dlc_read_reg(&ism330dlc_ctx, ISM330DLC_FIFO_CTRL5, &reg_val, 1);
 printf("FIFO_CTRL5: 0x%02X (Expected 0x66)\n", reg_val);
 ism330dlc_read_reg(&ism330dlc_ctx, ISM330DLC_INT1_CTRL, &reg_val, 1);
 printf("INT1_CTRL: 0x%02X (Expected 0x08)\n", reg_val);
}

void ISM330DLC_Configure(void) {
 // Enable accelerometer
 ISM330DLC_ACC_Enable(&ism330dlc_obj);
 ISM330DLC_ACC_SetOutputDataRate(&ism330dlc_obj, ISM330DLC_XL_ODR_6k66Hz); // 52 Hz
 ISM330DLC_ACC_SetFullScale(&ism330dlc_obj, ISM330DLC_16g); // ±2g

 // Enable gyroscope
 ISM330DLC_GYRO_Enable(&ism330dlc_obj);
 ISM330DLC_GYRO_SetOutputDataRate(&ism330dlc_obj, ISM330DLC_GY_ODR_6k66Hz); // 52 Hz
 ISM330DLC_GYRO_SetFullScale(&ism330dlc_obj, ISM330DLC_2000dps); // ±500 dps

 // Enable Block Data Update
 ism330dlc_block_data_update_set(&ism330dlc_ctx, PROPERTY_ENABLE);

 // Configure FIFO
 ISM330DLC_ConfigureFIFO();


 // Verify
 uint8_t reg_val;
 ism330dlc_read_reg(&ism330dlc_ctx, ISM330DLC_CTRL1_XL, &reg_val, 1);
 printf("CTRL1_XL: 0x%02X (Expected 0x90)\n", reg_val);
 ism330dlc_read_reg(&ism330dlc_ctx, ISM330DLC_CTRL2_G, &reg_val, 1);
 printf("CTRL2_G: 0x%02X (Expected 0x94)\n", reg_val);
}


//void ISM330DLC_ReadData(void) {
// ISM330DLC_Axes_t accel_data;
// ISM330DLC_Axes_t gyro_data;
//
// if (ISM330DLC_ACC_GetAxes(&ism330dlc_obj, &accel_data) == ISM330DLC_OK) {
// // printf("Accel: X=%ld, Y=%ld, Z=%ld mg\n", accel_data.x, accel_data.y, accel_data.z);
// printf("$%d %d %d;",accel_data.x, accel_data.y, accel_data.z);
// }
//
//// if (ISM330DLC_GYRO_GetAxes(&ism330dlc_obj, &gyro_data) == ISM330DLC_OK) {
//// printf("Gyro: X=%ld, Y=%ld, Z=%ld mdps\n", gyro_data.x, gyro_data.y, gyro_data.z);
//// }
//}

void ISM330DLC_ReadData(void) {
 uint16_t fifo_level;
 if (ism330dlc_fifo_data_level_get(&ism330dlc_ctx, &fifo_level) != 0) {
 return; // Error
 }

 if (fifo_level > 0) {
 // Each sample is 12 bytes (6 for accel, 6 for gyro)
 uint8_t buffer[12 * 100]; // Buffer for up to 100 samples
 uint16_t bytes_to_read = fifo_level * 12;

 if (ism330dlc_fifo_raw_data_get(&ism330dlc_ctx, buffer, bytes_to_read) == 0) {
 for (uint16_t i = 0; i < fifo_level; i++) {
 // Extract accel and gyro from buffer (16-bit per axis)
 int16_t accel_x = (int16_t)(buffer[i * 12 + 0] | (buffer[i * 12 + 1] << 8));
 int16_t accel_y = (int16_t)(buffer[i * 12 + 2] | (buffer[i * 12 + 3] << 8));
 int16_t accel_z = (int16_t)(buffer[i * 12 + 4] | (buffer[i * 12 + 5] << 8));
 int16_t gyro_x = (int16_t)(buffer[i * 12 + 6] | (buffer[i * 12 + 7] << 8));
 int16_t gyro_y = (int16_t)(buffer[i * 12 + 8] | (buffer[i * 12 + 9] << 8));
 int16_t gyro_z = (int16_t)(buffer[i * 12 + 10] | (buffer[i * 12 + 11] << 8));

 // Convert raw to physical units (example for ±2g and ±500 dps)
 float accel_x_mg = ISM330DLC_FROM_FS_2g_TO_mg(accel_x);
 float accel_y_mg = ISM330DLC_FROM_FS_2g_TO_mg(accel_y);
 float accel_z_mg = ISM330DLC_FROM_FS_2g_TO_mg(accel_z);
 float gyro_x_mdps = ISM330DLC_FROM_FS_500dps_TO_mdps(gyro_x);
 float gyro_y_mdps = ISM330DLC_FROM_FS_500dps_TO_mdps(gyro_y);
 float gyro_z_mdps = ISM330DLC_FROM_FS_500dps_TO_mdps(gyro_z);

 // Check for changes (optional threshold)
 #define CHANGE_THRESHOLD 10
 if (abs(accel_x_mg - prev_accel_data.x) > CHANGE_THRESHOLD ||
 abs(accel_y_mg - prev_accel_data.y) > CHANGE_THRESHOLD ||
 abs(accel_z_mg - prev_accel_data.z) > CHANGE_THRESHOLD) {
 printf("Accel: X=%.2f, Y=%.2f, Z=%.2f mg\n", accel_x_mg, accel_y_mg, accel_z_mg);
 prev_accel_data.x = accel_x_mg;
 prev_accel_data.y = accel_y_mg;
 prev_accel_data.z = accel_z_mg;
 }

 if (abs(gyro_x_mdps - prev_gyro_data.x) > CHANGE_THRESHOLD ||
 abs(gyro_y_mdps - prev_gyro_data.y) > CHANGE_THRESHOLD ||
 abs(gyro_z_mdps - prev_gyro_data.z) > CHANGE_THRESHOLD) {
 printf("Gyro: X=%.2f, Y=%.2f, Z=%.2f mdps\n", gyro_x_mdps, gyro_y_mdps, gyro_z_mdps);
 prev_gyro_data.x = gyro_x_mdps;
 prev_gyro_data.y = gyro_y_mdps;
 prev_gyro_data.z = gyro_z_mdps;
 }
 }
 }
 }
}

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    April 10, 2025

    Hi @AmrithHN ,

    We don't have an example available for this specific product, but you can look at those of LSM6DSL at this link.

    The FIFO of the two products works in the same way.

    Hope this helps!