ISM330DLC - question about SDx and SCx pins
Hello,
I would like to ask a question related to ISM330DLC device. I am using in my application this device using I2C communication between STM32. During review I just realized that I didn't connect the SDX ( pin 2 ) and SCX ( pin 3 ) to VCC or GND ( I have left them unconnected ). If this mistake is critical for functionality of the device and is a must or I can still be able to communicate with the sensor?
I plan to use it in the MODE 1 function.
Thank you in advance
Jacek Pieczaba