Skip to main content
Visitor II
May 24, 2022
Solved

Issue with Nucleo-L552ZE-Q and X-NUCLEO-IKS01A3 Are they compatible?

  • May 24, 2022
  • 1 reply
  • 835 views

I have downloaded all the needed software and st-link (and update) but Unicleo_GUI does not recognize the expansion board. In my device manager, the virtual COM is there. I am able to connect to the right port, but only if I tick the box that lists all the COM ports. Any help is much appreciated. Thanks

    This topic has been closed for replies.
    Best answer by Imen.D

    Hello @DLlam.1​ and welcome to the Community :)

    The X-NUCLEO-IKS01A3 is compatible with Nucleo-L552ZE-Q (with STM32 Nucleo boards)

    Maybe you have to check solder bridges.

    You can check if the available -ready to use- examples with STM32L5 are working.

    Make sure to include the IKS01A3 from the BSP folder under X-CUBE-MEMS package:

    STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\8.3.0\Drivers\BSP

    and Import the Components folder from X-CUBE-MEMS package: STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\9.2.0\Drivers\BSP\Components

    then, add it in the Components folder of the CubeL5 package:

    STM32Cube\Repository\STM32Cube_FW_L5_V1.4.0\Drivers\BSP\Components

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    Imen

    1 reply

    Imen.DAnswer
    Technical Moderator
    May 26, 2022

    Hello @DLlam.1​ and welcome to the Community :)

    The X-NUCLEO-IKS01A3 is compatible with Nucleo-L552ZE-Q (with STM32 Nucleo boards)

    Maybe you have to check solder bridges.

    You can check if the available -ready to use- examples with STM32L5 are working.

    Make sure to include the IKS01A3 from the BSP folder under X-CUBE-MEMS package:

    STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\8.3.0\Drivers\BSP

    and Import the Components folder from X-CUBE-MEMS package: STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\9.2.0\Drivers\BSP\Components

    then, add it in the Components folder of the CubeL5 package:

    STM32Cube\Repository\STM32Cube_FW_L5_V1.4.0\Drivers\BSP\Components

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    Imen