Issue with running X-CUBE-MEMSMIC1 (version 5.6.0), UltrasoundFFT on STEVAL-STWINKT1
Hello,
I am able to successfully compile X-CUBE-MEMSMIC1 (version 5.6.0), UltrasoundFFT for STM32L4R9ZI-STWIN (STEVAL-STWINKT1) - as Debug .bin file.
However, when I run it on the STWINKT1, the host Utility/GUI (UltrasoundFFT.exe) does not run. It is unresponsive when click the START button. Basically, the utility program hangs.
Alternatively, I don't have this problem when I use the compiled code from X-CUBE-MEMSMIC1 (version 5.5.0). It works fine.
I am wondering if anyone has tested this project (UltrasoundFFT for STWINKT1) using version 5.6.0? The Release Notes for version 5.6.0 says that "now using new GenericFFT library". I am wondering if there is any bug in this library (GenericFFTLibrary) versus the previous one used in version 5.5.0.
( I am using STM32CubeIDE version 1.9.0 on MS Windows 10, x64 PC for compiling.)
Thanks for any suggestion,