Skip to main content
Visitor II
July 26, 2022
Question

Issues with LSM6DSO Gyroscope Data

  • July 26, 2022
  • 1 reply
  • 776 views

As we are verifying the Gyroscope data output of the LSM6DSO, we noticed the value goes to -3.311157 randomly.

Below table is an example of the issue.

We are rotating the device at a constant speed and expected the value to be around 35, but all of a sudden, while the device is still rotating, we get a value of -3.311157.

Is there an known issue with the LSM6DSO?

Have there been an recent changes in the LSM6DSO?

0693W00000QMC5VQAX.png 

0693W00000QMC5fQAH.png 

Thank You!

    This topic has been closed for replies.

    1 reply

    ST Employee
    July 28, 2022

    Hi @KShah.2​ ,

    No, this is not a known issue. Are you facing this problem only on this LSM6DSO lot, or on just 1 part? You might check if I2C or SPI is stable during the communication.

    -Eleon