Skip to main content
Visitor II
September 19, 2019
Question

JTAG-20 to STDC14 adapter from ST for SensorTile.box

  • September 19, 2019
  • 3 replies
  • 4329 views

Hi all,

we recently got the SensorTile.box  which is a great toy. However we want to write our own applications and use the STDC14 debug connector. I just rread that only ST-LINK/V2 will be supported due to 1.8V debug interface.

Where can I get an adapter form Jtag-20 to STDC14 or 10-pin Cortex-M to STDC14.

ST offers this adapter as part of the SensorTile.box --> see page 3 here

Unfortunately this adapter and the cable was not part of the 2 SensorTile.boxes we received.

Does anyone know where to get the ST adapter or any adapter from 3rd Party supplier to convert to the STDC14 pinning?

Thanks!

    This topic has been closed for replies.

    3 replies

    ST Employee
    September 23, 2019

    Hi @Thilo​ , unfortunately the adapter is not yet available in the toolkit, It will be available soon (est. init Oct). If possible for you, I suggest to directly wire the ST LINK V2 pins to the STDC14 connector following the respective schematics as shown below. Regards

    0690X00000ARV7iQAH.png

    0690X00000ARV82QAH.png

    Thilo1Author
    Visitor II
    September 23, 2019

    Thanks @Eleon BORLINI​  for your reply.

    That's fine for me.

    As a workaround I used the 10-pin Cortex-M to 14-pin STDC cable from the STLINK-V3 and a separate JTAG 20-pin Adapter to connect to my STLINK/V2

    Visitor II
    February 7, 2020

    Hi @Thilo​ 

    Would it possible for you to provide the links for the connectors and adapters that you used/found.

    Thanks in advance

    Graduate II
    February 7, 2020

    The V3 KIT comes a collection of different cables (the mini does not). Basically a 10 conductor ribbon cable, a 10-pin header crimped on one end, a 14-pin header centre crimped on the other, with an empty pair at either end.

    Adapters, like this Olimex one could be used with the ST-LINK/V2

    https://www.olimex.com/Products/ARM/JTAG/ARM-JTAG-20-10/

    Visitor II
    February 7, 2020

    Dear @Eleon BORLINI​ ,

    I was wondering if there is a way to purchase the STDC 14 pin adapter mentioned above.

    I have recently purchased the Sensortile.box and the STLINK/V2 but non of the provided connectors are meant for the Sensortile.box

    Any help or guidance would be much appreciated.

    Thank you in advance