Question
L3GD20 DRDY stability
Posted on February 06, 2014 at 09:59
Hi,
I'm testing L3GD20 with SPI on my small test board. It looks like OK so I can get gyro data and DRDY signal with 760Hz. But when I monitor DRDY signal with my oscilloscope, it has a jitter sometimes. The difference is about plus-minus 10-20 uSec. It's not continuous jitter but 5 or 6 second each. I understand that L3GD20 has some time keeper to ADC the sensor with free running. So I cannot modify the interval (760Hz), right ? Are there any issue to get no jitter with software or hardware ? Best Regards, Zak #l3gd20-drdy-stability