Solved
L3gd20 sensor on stm32f411e-discovery
I am practicing reading L3GD20 data built into the stm32f411e-discovery kit. I use SPI1 to communicate with L3GD20. I watched on YouTube, they have instructions on how to use the void function HAL_GPIO_EXTI_Callback. I cannot call the void HAL_GPIO_EXTI_Callback function to read data from the sensor. Debug only receives the value from the bar but not the value read from the sensor
I use pin PE1 (configuration: Rising edge trigger detection, Pull-up ). Below is an image of my code. I need help.
Thanks everyone