Linearity of the LSM9DS1 gyro
Is there a number / measure for the linearity of the LSM9DS1 gyro across the 0-360deg range ?
I mean, how much 1deg measured at 0deg orientation is the same as 1deg measured at 90deg orientation ?
Thanks
Is there a number / measure for the linearity of the LSM9DS1 gyro across the 0-360deg range ?
I mean, how much 1deg measured at 0deg orientation is the same as 1deg measured at 90deg orientation ?
Thanks
The angular rate (the output of the accelerometer) is linear across the complete rotation, if the rotational speed is below the device full scale (for example, below +-245dps if this is the selected FS).
In principle, also the orientation angle is linear too. However, between the rate and the angle there is an integration procedure, and there are deviations from the theoretical behavior. The three most important factors are: the zero rate level (ZRL, offset), the noise level and the ODR parameters. The first accumulates during the integration procedure, so the indication is to perform at least a calibration of the offset at the beginning of the rotation. The noise should be less impacting, being on a variable around 0dps average. Last, the ODR determines the timebase for the integration operation, so you should calibrate it according to the speed of the movements you want to detect: for example, use low ODRs for slow movements.
-Eleon
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.