LIS25BA PCB + MKI109V3 Motherboard evaluation - WHO_AM_I register issues
I am having trouble evaluating a custom PCB with a LIS25BA accelerometer fitted.
The circuit is exactly the same as ST evaluation board for the same part (STEVAL-MKI211V1 + MKIGIBV3).
When connecting to the motherboard using the ST evaluation board, UNICO is able to connect to the device and all the data and registers are there as they should be (i.e who_am_i = 20h).
When using my own PCB connected to the same pins as the evaluation board the connection fails:
"ERROR: The adapter board has not been recognized.
The WHO_AM_I register value does not match the device selected"
Am I missing a software configuration step over I2C? Is the evaluation board configured to anything other than factory default?
Have I translated the interconnections incorrectly?
I would be grateful for some support on this matter.
Thank you.
Regards,
Robin