Skip to main content
Visitor II
January 8, 2018
Question

LIS2DE accelerometer drawing huge current - Power down mode not working

  • January 8, 2018
  • 1 reply
  • 610 views
Posted on January 08, 2018 at 08:08

Hi,  I am working on a custom board wherein, I am using  LIS2DE12  accelerometer. The custom board draws around 0.1mA current. After the removal of the accelerometer from the board, the board drwas only 3uA current. So, I  would like to disable the accelerometer operation for minimising the current consumption, and for this, after initialization, I am writing the power down command 0x00 to the register CTRL_REG1 (20h). But the accelerometer still draws 0.1-0.2mA current. Please suggest the possible reasons for the same.   

Thanks

#lis2de12 #accelerometer
    This topic has been closed for replies.

    1 reply

    ST Employee
    January 8, 2018
    Posted on January 08, 2018 at 16:40

    I suppose you connected the SA0 pin to GND and the current is drawn by this pin, because this pin has internal pull-up.