LIS2DE12 not reaching current consumption said in datasheet
Hello,
I'm evaluating the LIS2DE12 accelerometer by using the combination of STEVAL-MKI175V1 and STEVAL-MKI109V3 along a Power Profiler Kit II from Nordic Semiconductors for current measurement.
Method of test:
I removed the jumper that source VDD, bridged the Power Profiler Kit II (2 red circles) and connected GND (yellow circle)

Placed the STEVAL-MKI175V1 and connected it to the computer.

I proceeded to open UNICO-GUI and configured it to run at 200 Hz ODR with a range of 2g. Also enabled bit I1_ZYXDA from CONFIG_REG3 (22h) as I'm planning to catch the data available coming from INT1 in my application.

The datasheet describes that the expected consumption is 18 uA at 200 Hz ODR.

But the result leaded to a consumption of 41.36uA with an average consumption of 42.2uA. This is more than the double expected consumption.

Am I missing something to configure in order to achieve the expected consumption?