Skip to main content
Visitor II
December 23, 2017
Question

LIS2DE12 query related to #INT pins.

  • December 23, 2017
  • 2 replies
  • 845 views
Posted on December 23, 2017 at 05:47

Hello,

I am using LIS2DE12 Accelerometer in my device interfaced with 32 bit STM32L4 sereis.

Looking into the datasheet LIS2DE12 having two INT pins.

My question is do i need to interface both pins with micro controller or single pin will work keeping other pin open.

Application is Fleet Management System.

#mems #accelerometer #lis2de12 #gyro
    This topic has been closed for replies.

    2 replies

    Visitor II
    December 23, 2017
    Posted on December 23, 2017 at 07:18

    Yes, you can leave either or both interrupt pins open.

    ST Employee
    December 25, 2017
    Posted on December 25, 2017 at 09:35

    You have to decide which feature of the accelerometer you will use. Then you will know how many interrupt pins need to be connected to microcontroler. None of the interrupt pins have to be connected to microcontroler, it is not mandatory. But in example if you want to use data ready interrupt on INT1 and threshold interrupt on INT2 you have to connect both of them to the microcontroller.

    Visitor II
    January 4, 2018
    Posted on January 04, 2018 at 11:41

    Hi Miroslav

    Thanks your reply

    How 

    threshold interrupt is work?

     and how to use?

    please give me suggestion for that.

    Thanks 

    ST Employee
    January 4, 2018
    Posted on January 04, 2018 at 14:49

    Please read chapter 6 in

    http://www.st.com/content/ccc/resource/technical/document/application_note/77/ed/e7/e1/28/5a/45/d6/CD00290365.pdf/files/CD00290365.pdf/jcr:content/translations/en.CD00290365.pdf

     it describes the interrupts. The application note is for LIS3DH but the functionality of the threshold interrupts is basically the same.