LIS2DE12 self test
I am trying to set up a self test process for an assembly including an LIS2DE12. The device works normally when I tilt and invert it. When I try to put it in to self-test mode by writing either 02h or 04h to CTRL_REG4 the readings are the same as with 00h written to CTRL_REG4.
I initially tried using the process for the LIS3DH on Page 57 of AN3308 but that says to write 80h to CTRL_REG4, which does not seem to be valid because that would set the BDU bit to 1, not valid for an 8 bit part, and not set either of the self test bits.
Can someone please shed some light on whether the self-test function is available with the LIS2DE12 and what I can expect from it.
Thanks in advance,
Rob