Lis2dh App Scanrate and Speed of Lis2dh
Hello Ladies and Gents,
I have following Problem with my App:
The Scanrate from given Timer can be in min. 10ms. These ist f=1/0,010=100Hz.
So If I configure the Lis2dh to normal or Highres Mode I have a f=1.344 KHz
Anybody have an Idea how to increase/decrease the Scanrate to geht all the values of interval?
Also I'm bind to USB and the Transactiondelay from max 500ms.
Stv