Skip to main content
Visitor II
July 18, 2019
Question

LIS2DH power consumption with 1 axis enabled?

  • July 18, 2019
  • 1 reply
  • 863 views

We're evaluating the LIS2DH (and -DE) for a very low-power project, and every uA is precious. We only need readings from one axis, so I am curious as to whether disabling the other two axes would result in power savings. I've tried measuring it here on my desk, but sadly, my multimeter isn't sufficiently accurate down in the single-digit-uA range.

So my question is: does disabling one or more axes reduce the power consumption?

    This topic has been closed for replies.

    1 reply

    ST Employee
    July 19, 2019

    Hi @Community member​ , the answer to your question is basically no, i.e. the difference in terms of current consumption between a full-axis enabled configuration and a single axis configuration is negligible. The fact is that the internal electronics "stops" the data of the single axis just before the muxing with the other axis (ADC running and so on), but the output tri-state buffer is nevertheless active for the enabled axis. Regards