LIS2DH register details missing
Hi there,
I was working on the LIS2DH for one of our applications, and found that there are some details missing in the datasheet (Doc ID 022516 Rev 1), enlisted below:
1- The bits HPCF2 - HPCF1 in the CTRL_REG2 (21h) corresponding to the high pass filter cut off frequency selection do not have any details mentioned about how they affect the cut-off frequency.
2- The REFERENCE/DATACAPTURE (26h) also does not have any details about it mentioned in the datasheet, except that it acts as the reference for the HPF. What does the "Data Capture" here represent?
3- Also, there is no information about the various bits of the FIFO_SRC_REG (2Fh).
It would be really appreciable if you could share details on the functionality of these bits/registers.
Looking forward to hearing back from soon.
Warm regards,
Sarthak Malik.