LIS2DH12 consecutive Interrupt occur even though only one trigger
I use accelerometer LIS2DH12 to wake up the device by motion detection. It's working correctly for long time but currently I found a trouble with interrupt. It's rarely happen and hard to reproduce.
Here is my initialization:
INT1_CFG = 0010 1010
INT1_THS = 0000 0010
INT1_DURATION = 0000 00010
CTRL_REG2 = 0000 0101
CTRL_REG3 = 0100 0000
CTRL_REG5 = 0000 1010 (LIR_INT1 = 1)
read to clear INT1_SRC
I start up my device and wait device go to sleep, then I lightly touch on my device to wake up, The INT1 signal and I read INT1_SRC register before continue proccess. After that, the INT1 still signals again and again eventhough I leave my device stable on the table.
I have checked LIR_INT1 at CTRL_REG5 that INT1_SRC cleared by reading INT1_SRC but when INT1 signal, I read INT1_SRC (= 0110 1000 for example) then second read INT1_SRC (still = 0110 1000).
To stop INT1, I have to clear INT1_CFG in my code. Note that, The whole process I make sure that the device stay stable on the desk and only touch at the first time.